« Back Toshiba Brings Innovation to Industrial Waste Water Treatment System

Introduces its ecologically friendly Non-chemical Feed Filtration System at the upcoming Singapore International Water Week 2012

TOKYO—Toshiba Corporation (TOKYO: 6502) today announced that it will bring its Non-chemical Feed Filtration System, an innovative water treatment system that will offer the manufacturing sector a cost-efficient, environmentally friendly water treatment system, to Singapore International Water Week 2012.

Toshiba’s Non-chemical Feed Filtration System offers multiple benefits. As an environmentally conscious water treatment system that applies Toshiba’s unique functional powder[1] as a filter aid[2] it eliminates the coagulants[3] found in conventional water treatment systems, reducing residual waste, while The functional powder can be circulated and reused within the system, cutting the cost of treating waste water by approximately 40%[4].

The system has already been delivered to Fujitsu Limited’s printed circuit board plant in Nagano Japan, where it started operation this month. Toshiba also plans to introduce the system to factories in other Asian countries outside Japan, where there is a fast growing need for a water treatment technology that significantly cuts environmental burdens. The system will be on display at Singapore International Water Week 2012 (SIWW2012), to be held in Marina Bay Sands, Singapore, from July 2nd to 4th, 2012.

Conventionally, waste water containing minute suspended solids[5] and with a high specific filtration resistance is treated in a water treatment system that uses coagulants, such as the coagulation-sedimentation method or the dissolved-

air-floatation method. However, these conventional systems generate environmental loads, most notably concentrations of suspended solids in sludge, the direct result of the use of coagulant. Toshiba’s innovative system reduces waste generation, a critical issue in the context of industrial water treatment; cuts operating costs significantly; and allows recovery and reuse of valuable materials in the waste water.

The Non-chemical Feed Filtration System reduces the concentration of suspended solids in waste water without the use of any coagulant, by applying Toshiba’s functional powder as a filter aid to promote the removal of suspended solids. Using magnetism to separate the magnetic functional powder from the suspended solids achieves reductions in both the chemical-derived sludge and the cost of waste disposal, and also allows valuable substances in the suspended solids to be recovered with a high level of purity. Running costs are also substantially reduced, since the separated and recovered functional powder can be circulated and reused within the system.

“We are delighted to bring our innovative water treatment system to Singapore International Water Week 2012,” said Mr. Naohiro Noro. “Toshiba’s Non-chemical Feed Filtration offers high performance water treatment without the use of coagulants. It has already met the stringent requirements of Fujitsu, and we now plan to introduce it throughout Asia, where it can contribute to cost efficient operation and to environmental protection. We very much look forward to introducing it at International Water Week.”

At the Singapore International Water Week 2012, the global platform for the sharing and co-creation of water solutions, Toshiba will also showcase other water solutions and technologies, including its UV disinfection systems and ozone generator systems.

Toshiba will continue to create environmentally conscious products such as the Non-chemical Feed Filtration System and to promote business activities in industrial water treatment.

Notes:

[1] The functional powder applied in the system as a filter aid captures and recovers fine suspended solids. It can be recovered and reused in the system.

[2] The use of a filter aid for filtering waste water provides three benefits: greater clarification of treated water; no clogging of filters; and a higher filtration rate with greater filtration area.

[3] A coagulant is a chemical that promotes sedimentation of fine particles contained in waste water that are difficult to separate by force of gravity.

[4] In the case of installation at Fujitsu, Ltd. Nagano Plant.

[5] Suspended solids are particulate matter floating on or suspended in water. They are less than 2mm in diameter.

Fujitsu Ltd.’s Nagano Plant manufactures printed circuit boards (PCB). In treating waste water from the PCB manufacturing process, Toshiba’s water treatment system will reduce suspended solids originating from coagulant and recover highly pure copper.

For further information of the product, please click here

Press Release Available in these languages (PDF) »

More news in Toshiba

Toshiba and GE Vernova Sign MoU to advance carbon reduction and efficiency for gas...

Read

Toshiba Launches New SCiB™ 24V Battery Pack for Automotive and Industrial Use - ...

Read

Toshiba’s Heavy Ion Therapy System CI-1000 Wins Minister of Economy, Trade and ...

Read
Toshiba Brings Innovation to Industrial Waste Water Treatment System

Toshiba and naturenix Scale Up and Transition to Paid Battery Subscription Pilot f...

Read
2025