Battery Business
Energy Storage SCiBTM
Digital Infrastructure Solutions
Battery Business
Battery Business
Industrial Lithium-ion Battery
Securing our quantum future
Toshiba SCiB™ is a highly safe rechargeable battery with six outstanding characteristics. By using oxide-based materials (Lithium Titanium Oxide), SCiB™ is designed to prevent thermal runaway resulting from short circuiting caused by physical stress.
Furthermore, SCiB™ has various superior characteristics, including a long life exceeding 20,000 charge/discharge (0%~100%) cycles, rapid charging time of 6 minutes, input/output current densities comparable with capacitors, and operation at temperatures as low as -30°C.

Key Features
Performance At Low Temperature
Usable even at -30°C
High Input/Output
Large current for both input and output
Wide Effective SOC* Range
Available SOC range of 0 to 100%
Rapid Charging
Rapidly charges to about 80% of the capacity in 6 minutes
Safety
Low risk of fire or explosion
Long Life
Cycle life of 20,000 times or more
*20Ah cell level test result under fixed conditions
** SOC: State of Charge
Toshiba’s SCiB™ rechargeable battery used in various fields
SCiB™ is active in a wide range of industries and locations and in a wide range of fields.
Hybrid Electric Vehicles
The high input/output capability of SCiB™ makes it possible to efficiently store the large electric energy generated during deceleration and braking, improving fuel efficiency and reducing emissions.
Plug-in Hybrid Vehicles
Battery systems composed of small SCiB™ cells help realize safe, long-life, and rapidly rechargeable electric vehicles.
Automotive Starter Battery
Featuring high power and long life even at low temperature, SCiB™ is a replacement for automotive lead-acid batteries.
Cranes
SCiB™ allows cranes to efficiently use the large kinetic energy that is generated while freight containers are lowered, contributing to improving fuel efficiency and reducing emissions.
Electric Ships
The minimum battery space required by SCiB™ makes it possible to secure spacious cabin. SCiB™ enables efficient operations of electric ferries with a small quantity of batteries.
Electric Buses
Electric buses using SCiB™ can be charged in a short period of time, such as, while they are at a bus stop. A reduction in the quantity of batteries makes it possible to secure a spacious passenger cabin and reduce costs.
Hybrid Buses
SCiB™ allows buses and other large vehicles to efficiently convert large kinetic energy into electric energy.
Hybrid Trucks
While a truck is on a downward slope, SCiB™ efficiently recovers the regenerated energy so as to be able to assist in climbing an upward slope later, improving fuel economy. The recovered energy can also be used by an air conditioner and a refrigerator while the engine is idle.
Railway
SCiB™ is suitable for the electrification of diesel locomotives. It can also be used to provide electric energy while a train is running on non-electrified sections and even in the event of emergency.
AGVs and AMRs
SCiB™ eliminates battery replacement because of its outstanding rapid-charging performance, enabling unattended operations of automated guided vehicles (AGVs) and autonomous mobile robots (AMRs).
Electric Power Systems
Storage battery systems composed of long-life and high-reliability SCiB™ enables frequency regulation of power grids.
UPS
SCiB™ helps realize small, light uninterruptible power supply (UPS) systems, improving space utilization and reducing battery replacement costs.
IoT
SCiB™ enables safe, small battery systems to support the development of IoT infrastructure because of its outstanding characteristics, including its high input/output density close to that of capacitors, long life, and low-temperature operation.
Drones
While conventional drones require battery replacement, SCiB™ makes it possible to create new drones that eliminate the need for battery replacement.
Revolution in SCiB™
SCiB™ can be used in a wide range of applications, such as automotive, railway, industrial equipment, power equipment and power plants
Suzuki Motor Corporation
Mild Hybrid
This battery has been adopted for low-fuel- consumption technologies that effectively use regenerative energy at deceleration.
Solaris Bus & Coach S.A.
Fast charging electric bus
SCiB™ has been adopted by Solaris Bus & Coach S.A. for its fast charge electric bus in Europe.
Damen Shipyards
Power source for electric ferry
SCiB™ is used as the power source for the electric ferry which is designed and built by Damen Shipyards (Damen Ferry 2306E3).
Willey Battery Utility, LLC
Adjustment of electricity demand and supply
This battery has been adopted for large battery systems for adjustment of electricity demand and supply in the United States
Toshiba Infrastrucute Systems
Uninterruptible power supply (UPS)
This battery has been adopted for uninterruptible power supplies (UPS) that serve as backup power supplies for critical loads including small servers to large data centers.
Toshiba Elevator and Building Systems Corporation
Power-outage continuous operation function
This battery has been adopted for the elevator that moves continuously in the case of power outage.
Siemens AG
Traction power source for railway system “Mireo”
SIEMENS Mobility realizes high safety and long life system required for railway systems by using SCiB™ as a traction power source.
Shanghai Hi-tech Control System Co., Ltd. (HITE)
Battery system for Rubber Tired Gantry crane
The regenerative energy stored in the battery when the crane lowers can reuse when the crane hoists or moves the crane body by tires
Terna S.p.A in Italy
BESS for Frequency Regulation
Our system is highly valued as a solution that could realize stable grid by controlling
frequency and grid fluctuation.