From Dream to Reality: Toshiba and Airbus Drive the Future of Hydrogen-Powered Flight with Superconducting Motors

Superconducting Motor banner

While the aviation sector rushes to achieve net-zero CO₂ emissions by 2050, innovations beyond the limits of sustainable aviation fuel remain essential. This is where Toshiba’s superconducting motor fits: a compact, lightweight, and high-output solution for electric propulsion systems. With less than one-tenth of the weight and size of conventional 2MW-class motors, such a drastic reduction in size and weight represents a game-changer in aviation, where every kilogram matters, and high output is required.

Conventional vs Superconducting motor

Less than one-tenth the weight and smaller than other 2MW-class motors with the same output power

Recognizing the promise of the prototype motor, first presented in 2022, the world’s largest aircraft manufacturer, Airbus, began collaborative research in 2024 to further develop and scale this technology. The joint signing of the partnership agreement at Japan International Aerospace Expo 2024 underlining both companies’ determination to promote aerospace innovation. Building on over 50 years of experience in superconducting technology, this partnership brings together Toshiba’s and Airbus’s innovations in hydrogen propulsion and aircraft electrification programs and marks a pivotal step toward realizing zero-emission flight.

Aircraft with superconducting motor

An image of an aircraft equipped with a superconducting motor

Hydrogen-powered aircraft are set to transform air travel by replacing fossil fuels with clean energy solutions. Hydrogen can power aircraft in two ways: burning it in turbines or converting it to electricity in fuel cells. The second way is much more efficient, as it allows electric propulsion with zero CO₂ emissions. Toshiba’s superconducting motor amplifies this advantage by operating at cryogenic temperatures and, therefore, no electrical resistance, maximizing energy efficiency. Liquefied hydrogen stored at -253°C environment serves as both fuel and coolant, creating a perfect synergy that improves performance while reducing weight and paving the way for sustainable aviation.

Beyond aviation, Toshiba envisions superconducting motor technology as a powerful engine for sustainable mobility in various applications. Its lightweight, high-output design and cryogenic efficiency make it ideal for large-scale applications where weight and energy performance are critical. Potential future uses include powering next-generation ships for clean maritime transport and propulsion for space travel.

Toshiba combines technologies

Toshiba combines technologies to achieve a greater good

Toshiba and Airbus have taken a revolutionary path toward carbon-neutral skies, reshaping aviation with superconducting motors and hydrogen-powered propulsion systems. This collaboration goes beyond engineering; it embodies a vision of mobility free from carbon emissions while breaking through new efficiency frontiers. By pairing superconductivity with hydrogen’s potential as a clean energy source, the partnership is shaping a future where aircraft fly farther, cleaner, and smarter.

Read the full article HERE

More News in Toshiba

Enquiry for
From Dream to Reality: Toshiba and Airbus Drive the Future of Hydrogen-Powered Flight with Superconducting Motors

Enquiry for

This field is for validation purposes and should be left unchanged.
This field is hidden when viewing the form

Enquiry for

Business Strategy

Committed to People, Committed to the Future.

The Asia Pacific region is an important market for Toshiba, with one of the fastest-growing demands in infrastructure, energy, mobility, and connectivity.
Message from Managing Director

Securing Sensitive Information with Quantum Key Distribution

At Toshiba, we’re committed to delivering world leading technology that protects the private information of citizens and organizations.

Discover how Toshiba cutting edge quantum technology can protect the sensitive information of financial institutions.

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

Solutions Map - A data-connected society by Toshiba

Solutions map illustrating Toshiba’s vision for a connected data-driven society

Navigate the interactive solution map to witness the full scope of Toshiba’s integrated solutions. By connecting data across systems, we deliver comprehensive, tailored outcomes for a smarter and more sustainable future.

Our Contributions - Sustainable Activities

Technology Spotlight

Toshiba Power Semiconductor

Toshiba leverages its 60 years expertise in power semiconductors to drive automotive electrification and sustainability, offering innovative solutions to enhance efficiency and reduce emissions across industries.

Quantum Key Distribution (QKD)

Building a quantum-secure future with Toshiba’s Quantum Key Distribution

Toshiba's Commitment to a Carbon-Neutral Future

With innovative technologies and a deep commitment to building a better world, Toshiba is working towards stable, efficient green energy infrastructures for a Carbon-Neutral Future.

Superconducting Motor

Toshiba Superconducting Motor has revolutionized the airline and transportation industries. It is lightweight, compact and high-Power, making it possible to replace fossil-fuel-driven engines and contributing to zero-emissions for various types of large mobility vehicles.

The Essence of Toshiba

Our philosophy section highlighting company values and guiding principles

Basic Commitment Of The Toshiba Group

Committed to People,
Committed to the Future.

At Toshiba, we commit to raising the quality of life
for people around the world. ensuring progress
that is in harmony with our planet

Our Purpose

We turn on the promise of a new day.

Our Values

Do the right thing. Look for a better way.
Always consider the impact. Create together.