Generating Power from a Waterfall Only as Tall as a Man: Micro Hydro Broadens the Appeal of Hydropower

Mounting concerns about environment degradation are accelerating adoption of many and various renewable energy systems around the world, with solar, wind, and biomass power among the more familiar. However, the largest single source of emission-free, renewable electricity worldwide is hydroelectric power, which harnesses the power of moving water to generate electricity.

The key advantages of hydropower are minimal CO2 emissions and outstanding energy conversion efficiency. But major facilities that rely on huge dams on major rivers have long been the predominant source of hydropower, impeding widespread take-up of this form of renewable energy.

In the economics of hydropower projects, the cost of facilities for the water intake, pipelines and other equipment looms larger than that of the actual power generation facilities, the hydro turbines and generators. This high cost is a major disincentive, one that Toshiba is working to overcome through various development measures. Most notable of these is combining hydro turbines and generators in Hydro-eKIDS™, an easily installed, ultra-compact hydro turbine-generator unit suitable for virtually any site. The telling feature of Hydro-eKIDS™ is that a hydraulic head of only two meters is enough for it to generate electricity.

Micro Hydro Broadens the Appeal of Hydropower

Ultra-compactness makes the impossible possible
Hydro-eKIDS™ has a long history: the first unit was delivered in 2001 for a project on Lombok in Indonesia. It was initially positioned as a power generator for non-electrified areas.

Subsequently, however, demand for micro hydropower generating equipment unexpectedly soared in Japan, on factors including adoption of the Kyoto Protocol and concerns about electricity supply in the aftermath of major earthquakes. Use of the equipment in low-head locations, including those where industrial wastewater or household wastewater produced a sufficient flow, were a revolutionary step beyond traditional micro hydropower applications, which typically relied on flows from irrigation systems, industrial water, and river maintenance discharge. This greatly broadened the appeal of hydropower.

Toshiba has also used the compactness of the equipment to explore real innovations in application. One example is the use of water circulating in an air-conditioning system at a school in Tokyo, where electricity is generated by mounting equipment on existing piping. A pump circulates water between a heat exchanger installed on the roof of the school building and a tank installed under the building, producing chilled water in summer and hot water in winter. Although the circulating pump runs on late-night power, the system generates electricity by using the hydraulic head created by the drop from the rooftop heat exchanger to the underground tank. The electricity generated is used to illuminate the school lobby.

Hydro-eKIDS™ is uniquely suited

Hydro-eKIDS™ is uniquely suited to such initiatives to use modest amounts of water power to generate electricity. In the case of the school, in addition to the practical utility of the system, the adoption of renewable energy in an educational setting helps to impart an informed awareness of environmental issues in young people who will exercise leadership in the future.

Since locations with the potential for micro hydropower generation include sites with large variations in the head and flow rates of water, Toshiba has also developed a variable speed power generation system that allows the turbine rotation speed to be adjusted over a wide range. This is expected to further expand the range of application.

Electricity Generated Locally, Consumed Locally Toshiba envisions a society where electricity produced using local water power is utilized in the community and powers the local economy, in short, locally generated electricity for local consumption. The key is small-scale, convenient and community-based.

Many locations where hydroelectric power facilities could be installed lack power transmission lines and other equipment, and construction proposals are sometimes abandoned because construction of transmission facilities would not be cost-effective. In cases like this, Toshiba is considering power supply involving hydrogen instead of power transmission lines.

Toshiba’s objective is to realize reliable systems that generate sufficient electricity in ways that are attuned to the needs and aspirations of users. Enhancement of a diverse line-up of power systems capable of satisfying the full spectrum of needs will contribute to the realization of a more convenient and secure society.

Highlights Available in these languages (PDF) »

More News in Toshiba

Enquiry for
Generating Power from a Waterfall Only as Tall as a Man: Micro Hydro Broadens the Appeal of Hydropower

Enquiry for

This field is for validation purposes and should be left unchanged.
This field is hidden when viewing the form

Enquiry for

Business Strategy

Committed to People, Committed to the Future.

The Asia Pacific region is an important market for Toshiba, with one of the fastest-growing demands in infrastructure, energy, mobility, and connectivity.
Message from Managing Director

Securing Sensitive Information with Quantum Key Distribution

At Toshiba, we’re committed to delivering world leading technology that protects the private information of citizens and organizations.

Discover how Toshiba cutting edge quantum technology can protect the sensitive information of financial institutions.

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

Solutions Map - A data-connected society by Toshiba

Solutions map illustrating Toshiba’s vision for a connected data-driven society

Navigate the interactive solution map to witness the full scope of Toshiba’s integrated solutions. By connecting data across systems, we deliver comprehensive, tailored outcomes for a smarter and more sustainable future.

Our Contributions - Sustainable Activities

Technology Spotlight

Toshiba Power Semiconductor

Toshiba leverages its 60 years expertise in power semiconductors to drive automotive electrification and sustainability, offering innovative solutions to enhance efficiency and reduce emissions across industries.

Quantum Key Distribution (QKD)

Building a quantum-secure future with Toshiba’s Quantum Key Distribution

Toshiba's Commitment to a Carbon-Neutral Future

With innovative technologies and a deep commitment to building a better world, Toshiba is working towards stable, efficient green energy infrastructures for a Carbon-Neutral Future.

Superconducting Motor

Toshiba Superconducting Motor has revolutionized the airline and transportation industries. It is lightweight, compact and high-Power, making it possible to replace fossil-fuel-driven engines and contributing to zero-emissions for various types of large mobility vehicles.

The Essence of Toshiba

Our philosophy section highlighting company values and guiding principles

Basic Commitment Of The Toshiba Group

Committed to People,
Committed to the Future.

At Toshiba, we commit to raising the quality of life
for people around the world. ensuring progress
that is in harmony with our planet

Our Purpose

We turn on the promise of a new day.

Our Values

Do the right thing. Look for a better way.
Always consider the impact. Create together.