Harnessing the Power of Renewable Energy — Electricity and Energy Storage

Original article is hosted here.

From the threat of natural disasters to climate change, there are many good reasons behind today’s calls to step up use of renewable energy. But power generated by the sun and wind is volatile, intermittent and variable over time. One promising approach is to harness the potential of energy storage technologies. We will take a look at some of those technologies and how they can accelerate the use of renewable power.

What’s the problem with storing electricity?

By its nature, electricity moves so fast that it reaches consumers as soon as it is generated.

Ampère’s circuital law explains how electricity flows and the relationship between an electric current and a magnetic field. An electricity flow is the propagation of electromagnetic waves made up of electric and magnetic fields. The movement of an electric charge generates a magnetic field(*1), and they are alternately propagated due to changes in the strength or direction of electric fields. Magnetic and electric fields are thus alternately propagated as an electromagnetic wave.

(*1) A magnetic field refers to the space around a magnet or similar object that is experiencing magnetism. An electric field refers to the space where voltage is applied.

Electricity and Energy Storage

Schematic of electromagnetic waves

The different types of electromagnetic waves include light, x-rays and electricity. In a vacuum, electromagnetic waves propagate at the speed of light, 300,000km per second.

In a power plant, an electromagnetic rotor is turned inside a series of coils, the stator, and the rotation induces electric current that is sent to us along power lines instantaneously.

Electricity and Energy Storage

Power plants produce electric power.

How can electricity be stored?

Today, technologies for storing electric energy in various forms are being studied and developed. The aim is to prevent power outages and to contribute to the utilization of renewable energy. We focus on two of them.

There are a wide variety of electrical energy storage methods.

There are a wide variety of electric energy storage methods. One is pumped hydroelectric energy storage (PHES). While it generates electric power, it also serves as a full-fledged power storage technology.It does this by storing water in an upper reservoir, as mechanical potential energy that can be used to meet high electricity demand. Released into a pipe, a penstock, it flows downhill to a lower reservoir with enough force to drive water turbines and power generators. During low electricity demand, surplus energy is used to pump the water from the lower reservoir back to the upper reservoir. For example, if a PHES power plant with four 400-megawatt turbines operates for eight consecutive hours, it can generate electricity equivalent to the daily energy consumption of nearly 1.6 million households(*2).

(*2) Source; Federation of Electric Power Companies of Japan in 2015

Mechanism of pumped hydroelectric energy storage

Mechanism of pumped hydroelectric energy storage

Toshiba is a long-established leader in PHES technologies, and the originator of one of the sector’s most important technology advances, the world’s first adjustable-speed PHES system. Adjustable speed means that, during both generation and pumping operation, electric power from and to a PHES system can be controlled in response to the change of grid frequency, the latter achieved by rotational speed adjustment of the generator motor of the PHES system. Adjustable-speed PHES systems contribute to more efficient operation and improved power grid stability.

Adjustable-speed generator motor No. 4 at the Kazunogawa Power Station, Japan

Adjustable-speed generator motor No. 4 at the
Kazunogawa Power Station, Japan

Another technology is rechargeable batteries. You may be familiar with these as storage batteries for smartphones.

Reachargable batteries are an electrochemical energy storage solution. They do not store electricity such as —when the anode material in the positive electrode and the cathode material in the negative electrode are immersed in electrolyte, an electrochemical reaction occurs that discharges electric energy. A reverse electrochemical reaction, charging, occurs when electricity is applied from an external source. This restores the anode and cathode materials to their respective states before discharge and allows repeated use.

Toshiba’s SCiB™ rechargeable battery

Toshiba’s SCiB™ rechargeable battery

Apart from these two technologies, research and development efforts are underway for many different energy storage technologies, including hydrogen energy storage system using fuel cells that chemically convert hydrogen and oxygen energy into electric energy.

These innovations are creating a broad range of energy storage technologies that support our lifestyles by mitigating disruptions in the demand-supply balance that can cause power outages. Energy storage brings more flexibility to the power grid by helping grid operators to manage variable energy resources such as wind and solar.

Highlights Available in these languages (PDF) »

More News in Toshiba

Enquiry for
Harnessing the Power of Renewable Energy — Electricity and Energy Storage

Enquiry for

This field is for validation purposes and should be left unchanged.

Enquiry for

Business Strategy

Committed to People, Committed to the Future.

The Asia Pacific region is an important market for Toshiba, with one of the fastest-growing demands in infrastructure, energy, mobility, and connectivity.
Message from Managing Director

Securing Sensitive Information with Quantum Key Distribution

At Toshiba, we’re committed to delivering world leading technology that protects the private information of citizens and organizations.

Discover how Toshiba cutting edge quantum technology can protect the sensitive information of financial institutions.

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

Solutions Map - A data-connected society by Toshiba

Solutions map illustrating Toshiba’s vision for a connected data-driven society

Navigate the interactive solution map to witness the full scope of Toshiba’s integrated solutions. By connecting data across systems, we deliver comprehensive, tailored outcomes for a smarter and more sustainable future.

Our Contributions - Sustainable Activities

Technology Spotlight

Toshiba Power Semiconductor

Toshiba leverages its 60 years expertise in power semiconductors to drive automotive electrification and sustainability, offering innovative solutions to enhance efficiency and reduce emissions across industries.

Quantum Key Distribution (QKD)

Building a quantum-secure future with Toshiba’s Quantum Key Distribution

Toshiba's Commitment to a Carbon-Neutral Future

With innovative technologies and a deep commitment to building a better world, Toshiba is working towards stable, efficient green energy infrastructures for a Carbon-Neutral Future.

Superconducting Motor

Toshiba Superconducting Motor has revolutionized the airline and transportation industries. It is lightweight, compact and high-Power, making it possible to replace fossil-fuel-driven engines and contributing to zero-emissions for various types of large mobility vehicles.

The Essence of Toshiba

Our philosophy section highlighting company values and guiding principles

Basic Commitment Of The Toshiba Group

Committed to People,
Committed to the Future.

At Toshiba, we commit to raising the quality of life
for people around the world. ensuring progress
that is in harmony with our planet

Our Purpose

We turn on the promise of a new day.

Our Values

Do the right thing. Look for a better way.
Always consider the impact. Create together.