High-Tech Road Solutions to Keep Vietnam Moving Forward

Against the backdrop of globalization, Japan, through its capabilities and experience in social infrastructure technology, is contributing to enhancing the infrastructure of countries undergoing rapid economic growth. One example is Vietnam, whose GDP per capita growth since 1990 has been among the fastest in the world. 

In Vietnam, a 1,811-kilometer north-to-south expressway is under construction. A 55-kilometer section to the east of Ho Chi Minh City, which connects Ho Chi Minh City to the key industrial city of Dong Nai province, shortens the usual three-hour journey between the two places to one hour. This stretch of the highway will feature an intelligent transportation systems (ITS) conceived and installed by a Japanese consortium.

The ITS system for Vietnam Expressway Corporation is but one fruit of a consortium of Japanese companies led by Toshiba. This is the first comprehensive ITS solution put together by Japanese companies for an overseas customer. The equipment had been tested and installed, and then officially opened to the public in Mar., 2017.

High-Tech Road Solutions to Keep Vietnam Moving Forward

Integrated solutions to enable a smoother road-use experience

Motorbikes, mainly commuter bikes, have long been the dominant form of private transportation in Vietnam. But the country’s rapid economic growth means they are increasingly sharing limited road space with growing numbers of cars, SUVs and so on. With Vietnam’s roads already thronged with traffic, congestion and gridlock are everyday realities for long-suffering road users in the bustling country. So, bringing the transportation system up to speed through the addition of more and better roads, including expressways, subways, and other transportation infrastructure, is a pressing national priority.

“Toshiba has more than 50 years of experience in road projects,” explains Atsushi Kawami (Highway & Traffic Solutions Engineering Dept., Social Systems Div., Infrastructure Systems & Solutions Company, as of June 30, 2017). “But, the maturity of the Japanese market has prompted us to seek new growth opportunities overseas. Our market surveys revealed the high potential of Vietnam where major road projects are gaining traction.”

According to Mr. Kawami, Vietnam’s massive plan for road construction is an opportunity for Toshiba’s total solutions incorporating traffic management and toll collection systems.

“At the heart of an ITS is cutting-edge information processing technology for integrated processing of information on people, roads, vehicles, and so on to reduce the disruption along road networks and inconvenience to their users—traffic backups, accidents, and other glitches,” explains Mr. Kawami, warming to his theme. “ITS consist of various subsystems, including those for traffic control and toll collection. In this project, the consortium is responsible for every element of the system, whether central or peripheral, for the 55-kilometer stretch of expressway.”

High-Tech Road Solutions to Keep Vietnam Moving Forward

The project involves toll collection system including ETC, and installing vehicle detectors for measuring traffic flows and automatically sensing backups at 52 points. Additionally, cameras are installed to monitor 16 areas, sensors to assess weather conditions, and wireless communications equipment for use by the technicians supervising the expressway.

Overcoming differences to make a positive future

Traffic management system is familiar in Japan and consequently there is a critical mass of expertise on which to draw. However, this is not the case for some overseas markets such as Vietnam. Despite certain obstacles, some unforeseen, project members took this positively.

High-Tech Road Solutions to Keep Vietnam Moving Forward

“I think the strength of Japanese companies is their strict quality awareness.” Mr. Kawami recalls. “We are also to look at the bigger picture and make comprehensive judgement. In addition, Toshiba has the relevant know-how which comes from more than 50 years of experience in road projects. The strengths of Vietnamese companies, on the other hand, are their efficiency and resilience. Because of a young, dynamic work force, Vietnamese members were able to come up with ideas that we couldn’t – for example, they decided on the place to set monitor cameras using drones.”

To make most of the strengths of both countries, the project members tried to optimize work allocation. For example, while Japanese staff designed the software of the central control system, which is the heart of the system, Vietnamese staff took initiative to design and procure the hardware and peripheral systems. This enabled a high-quality comprehensive system that is suitable for Vietnam to be installed as per the schedule and cost-effectively. The system also facilitates maintenance, which is essential for a system meant to be used for a long time.

High-Tech Road Solutions to Keep Vietnam Moving Forward

Mr. Kawami is excited about the future: “Going forward, the progress of ICT seems certain to continue, which means, for example, improvements in locational accuracy via GPS and faster information transmission. Eventually, I expect to see big advances in road infrastructure due to more accurate demand forecasts through big data analytics, as well as other game-changing technologies. It will be wonderful if we can contribute to the safety and security of people around the world by helping improve road networks, which are fundamental to well-being and prosperity.”

Certainly, success in Vietnam can be a stepping stone to a greater success for Japanese companies seeking to address burgeoning demand for social infrastructure in emerging economies.

  • Summary

1,811-kilometer expressways are under construction in Vietnam. The ITS package developed by Japanese companies has been adopted along a 55-kilometer section of the expressway. Such state-of-the-art expressway traffic management systems are vitally important social infrastructure for emerging-market countries.

Highlights Available in these languages (PDF) »

More News in Toshiba

Enquiry for
High-Tech Road Solutions to Keep Vietnam Moving Forward

Enquiry for

This field is for validation purposes and should be left unchanged.

Enquiry for

Business Strategy

Committed to People, Committed to the Future.

The Asia Pacific region is an important market for Toshiba, with one of the fastest-growing demands in infrastructure, energy, mobility, and connectivity.
Message from Managing Director

Securing Sensitive Information with Quantum Key Distribution

At Toshiba, we’re committed to delivering world leading technology that protects the private information of citizens and organizations.

Discover how Toshiba cutting edge quantum technology can protect the sensitive information of financial institutions.

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

Solutions Map - A data-connected society by Toshiba

Solutions map illustrating Toshiba’s vision for a connected data-driven society

Navigate the interactive solution map to witness the full scope of Toshiba’s integrated solutions. By connecting data across systems, we deliver comprehensive, tailored outcomes for a smarter and more sustainable future.

Our Contributions - Sustainable Activities

Technology Spotlight

Toshiba Power Semiconductor

Toshiba leverages its 60 years expertise in power semiconductors to drive automotive electrification and sustainability, offering innovative solutions to enhance efficiency and reduce emissions across industries.

Quantum Key Distribution (QKD)

Building a quantum-secure future with Toshiba’s Quantum Key Distribution

Toshiba's Commitment to a Carbon-Neutral Future

With innovative technologies and a deep commitment to building a better world, Toshiba is working towards stable, efficient green energy infrastructures for a Carbon-Neutral Future.

Superconducting Motor

Toshiba Superconducting Motor has revolutionized the airline and transportation industries. It is lightweight, compact and high-Power, making it possible to replace fossil-fuel-driven engines and contributing to zero-emissions for various types of large mobility vehicles.

The Essence of Toshiba

Our philosophy section highlighting company values and guiding principles

Basic Commitment Of The Toshiba Group

Committed to People,
Committed to the Future.

At Toshiba, we commit to raising the quality of life
for people around the world. ensuring progress
that is in harmony with our planet

Our Purpose

We turn on the promise of a new day.

Our Values

Do the right thing. Look for a better way.
Always consider the impact. Create together.