Introducing Quantum Cryptography: The What, When and How

Quantum Cryptography

Original article is hosted here.

At a time when technological advances have created an almost constant state of data proliferation, the need for the secure transmission of sensitive information has never been more significant. In fact, Cisco predicts mobile data traffic to increase sevenfold between 2016 and 2021*1. IT decision-makers evidently recognise this challenge, with the latest research from Toshiba revealing that, for over half (52%) of businesses in Europe, data security is a top three investment priority for the year ahead. Yet despite this, businesses often fall behind in keeping themselves aware and ahead of cyber-security trends and developments.

Enter quantum cryptography, which, by harnessing the principles of quantum physics, has the ability to usher in a new age of secure online communication. But what exactly is quantum cryptography, what problems does it solve, and how can it fill the gaps in online defences to enable businesses to stay one step ahead of any complex threats, now and in the future?

How does quantum cryptography work?

“Simply put, quantum cryptography provides a secure means for generating and distributing secret keys between two parties on an optical network,” says Dr. Andrew Shields, Assistant Managing Director at Toshiba’s Research Laboratory in Cambridge. “By harnessing the inherent unpredictability in the state of particles, like electrons or photons, quantum cryptography can be used to generate the random numbers needed for cryptographic applications. Furthermore, by sending streams of encoded single photons through an optical communication network, it is possible to share a secret digital key that can be used for encrypting or authenticating information.”

Dr. Andrew Shields, Assistant Managing Director at Toshiba’s Research Laboratory in Cambridge

Dr. Andrew Shields, Assistant Managing Director at Toshiba’s Research Laboratory in Cambridge

Why do we need it? Quantum cryptography now and in the future

It is widely considered today that public key encryption is an essential part of data security, but that’s being challenged by new attack strategies and the emergence of quantum computers that will ultimately render much of today’s encryption unsafe. Today’s security challenges and tomorrow’s security fears are driving the adoption of reliable quantum cryptography solutions and services to enable better data security.

Quantum cryptography now and in the future

As a result, the global quantum cryptography market is forecast to grow from USD 285.7 Million in 2017 to USD 943.7 Million by 2022, a CAGR of 27%*2. Yet quantum cryptography’s arrival is not as close to fruition nor as widely acknowledged within relevant fields. This doesn’t detract from its essential and unparalleled value as we move into the quantum age, so how far away from quantum cryptography are we, and what needs to be progressed in order to achieve this?

When will it reach the mainstream?

While not yet commercially available, scientists are now at the stage of being able to deploy the technology and demonstrate its benefits. Toshiba’s Cambridge Research Laboratory recently published a paper explaining a breakthrough made using a protocol known as Twin-Field QKD, extending the range of QKD to over 500 kilometres of standard telecom fibre.

“This opens up the potential for secure communication between cities such as London, Paris, Dublin, Manchester and Amsterdam. Beyond this, a number of large collaborative projects such as the Innovate UK EQUIP project and the EU Commission’s Horizon 2020 programme are also working to develop the technology and make QKD an accessible, valuable tool for the enterprise,” Dr. Shields said.

Beyond the desire for IT decision makers to keep their data secure when in transit from A to B, so too is legislation changing to make it the law that data concerning a person’s identity is kept safe, with the General Data Protection Regulation (GDPR) a prime example of this. Coupled with growing and diversifying cyber threats and the difficulties associated with data security, as well as the need for a new standard in protecting such information, QKD can be the pivotal tool in making sure data is kept safe and secure.

Toshiba’s Quantum Encryption System

Toshiba’s Quantum Encryption System

Planning for the future

Quantum cryptography has great potential to become the key technology for protecting communication infrastructure from cyber-attacks and putting businesses on the front foot when it comes to protecting operation-critical information. Unlike other existing security solutions, quantum cryptography is secure from all future advances in mathematics and computing, even from the number crunching abilities of a quantum computer. Standardisation of QKD protocols remains essential for commercialised quantum cryptography. The need to enable interoperability of technologies, develop the components market as well as processes and technology, will reduce the costs of creation and deployment of QKD and see the commencement of a more secure future for all of us.

Highlights Available in these languages (PDF) »

More News in Toshiba

Enquiry for
Introducing Quantum Cryptography: The What, When and How

Enquiry for

This field is for validation purposes and should be left unchanged.

Enquiry for

Business Strategy

Committed to People, Committed to the Future.

The Asia Pacific region is an important market for Toshiba, with one of the fastest-growing demands in infrastructure, energy, mobility, and connectivity.
Message from Managing Director

Securing Sensitive Information with Quantum Key Distribution

At Toshiba, we’re committed to delivering world leading technology that protects the private information of citizens and organizations.

Discover how Toshiba cutting edge quantum technology can protect the sensitive information of financial institutions.

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

Solutions Map - A data-connected society by Toshiba

Solutions map illustrating Toshiba’s vision for a connected data-driven society

Navigate the interactive solution map to witness the full scope of Toshiba’s integrated solutions. By connecting data across systems, we deliver comprehensive, tailored outcomes for a smarter and more sustainable future.

Our Contributions - Sustainable Activities

Technology Spotlight

Toshiba Power Semiconductor

Toshiba leverages its 60 years expertise in power semiconductors to drive automotive electrification and sustainability, offering innovative solutions to enhance efficiency and reduce emissions across industries.

Quantum Key Distribution (QKD)

Building a quantum-secure future with Toshiba’s Quantum Key Distribution

Toshiba's Commitment to a Carbon-Neutral Future

With innovative technologies and a deep commitment to building a better world, Toshiba is working towards stable, efficient green energy infrastructures for a Carbon-Neutral Future.

Superconducting Motor

Toshiba Superconducting Motor has revolutionized the airline and transportation industries. It is lightweight, compact and high-Power, making it possible to replace fossil-fuel-driven engines and contributing to zero-emissions for various types of large mobility vehicles.

The Essence of Toshiba

Our philosophy section highlighting company values and guiding principles

Basic Commitment Of The Toshiba Group

Committed to People,
Committed to the Future.

At Toshiba, we commit to raising the quality of life
for people around the world. ensuring progress
that is in harmony with our planet

Our Purpose

We turn on the promise of a new day.

Our Values

Do the right thing. Look for a better way.
Always consider the impact. Create together.