Toshiba takes on the world’s smallest LiDAR – Improving the “Eyes” of Autonomous Driving

Toshiba’s LiDAR with two newly developed projectors

Over the past decade, autonomous driving has progressed from a vision of the future to reality. LiDAR (Light Detection and Ranging, Laser Imaging Detection and Ranging) is an essential sensor for automated driving. The technology is available in some luxury cars with Level 3 conditional driving automation. Toshiba is among the companies with a LiDAR that can handle Level 4 autonomous driving.

Toshiba has recently revealed significant advances in the new palm-sized laser projector unit that pushes LiDAR’s detection range out to 300m, the world’s longest with an industry-leading image resolution of 1200×84 pixels. It can be configured with flexible combinations of projector units to handle a variety of long-range and wide-angle detection applications. This new LiDAR will advance progress in many application areas, such as autonomous driving and infrastructure monitoring, and opens the way to exploring partnerships in other areas.

Toshiba’s LiDAR with two newly developed projectors

Road safety is often compromised by poor weather and risks from events or disasters. The current use of surveillance camera and radar have limitation in measuring distance, is weak in capturing objects in 3D clearly, and has poor performance under low light conditions. Toshiba LiDAR systems instantly and accurately detect road conditions and support decision-making on movement. With decades of experience in semiconductors and our expertise in optical technologies, Toshiba is capable of realizing solid-state LiDAR’s miniaturization while at the same time ensuring reliability and durable performance.

Toshiba’s solution is a LiDAR that can use multiple small projector units, the laser beam source. They all emit an eye-safe beam in the same direction, which increases the effective range. This approach also keeps down the LiDAR’s overall size with shrinking the volume of the projector unit to 71cm3. The innovative circuit design reduces the motor control board by 60% against the size of the previous prototype and uses know-how in 3D component mounting to reposition components and lenses.

LiDAR is closely associated with vehicle automation, a fast-growing market expected to reach 42 million units a year by 2030. Toshiba aims to commercialize LiDAR for autonomous driving and high-precision infrastructure monitoring in the fiscal year 2023, and look forward to exploring new applications in robots, drones, and security devices.

Akihide Sai, Senior Research Scientist, IoT Edge Laboratory, 
Information and Communications Platform Laboratories, 
Corporate Research & Development Center, Toshiba Corporation

Higher image quality confirmed using LiDAR with two projectors (right) than one (left)

For the Press Release, please click here.

For the technology-related articles, please visit Toshiba Clip LiDAR (Part 1), LiDAR (Part 2).

Highlights Available in these languages (PDF) »

More News in Toshiba

Enquiry for
Toshiba takes on the world’s smallest LiDAR – Improving the “Eyes” of Autonomous Driving

Enquiry for

This field is for validation purposes and should be left unchanged.

Enquiry for

Business Strategy

Committed to People, Committed to the Future.

The Asia Pacific region is an important market for Toshiba, with one of the fastest-growing demands in infrastructure, energy, mobility, and connectivity.
Message from Managing Director

Securing Sensitive Information with Quantum Key Distribution

At Toshiba, we’re committed to delivering world leading technology that protects the private information of citizens and organizations.

Discover how Toshiba cutting edge quantum technology can protect the sensitive information of financial institutions.

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

Solutions Map - A data-connected society by Toshiba

Solutions map illustrating Toshiba’s vision for a connected data-driven society

Navigate the interactive solution map to witness the full scope of Toshiba’s integrated solutions. By connecting data across systems, we deliver comprehensive, tailored outcomes for a smarter and more sustainable future.

Our Contributions - Sustainable Activities

Technology Spotlight

Toshiba Power Semiconductor

Toshiba leverages its 60 years expertise in power semiconductors to drive automotive electrification and sustainability, offering innovative solutions to enhance efficiency and reduce emissions across industries.

Quantum Key Distribution (QKD)

Building a quantum-secure future with Toshiba’s Quantum Key Distribution

Toshiba's Commitment to a Carbon-Neutral Future

With innovative technologies and a deep commitment to building a better world, Toshiba is working towards stable, efficient green energy infrastructures for a Carbon-Neutral Future.

Superconducting Motor

Toshiba Superconducting Motor has revolutionized the airline and transportation industries. It is lightweight, compact and high-Power, making it possible to replace fossil-fuel-driven engines and contributing to zero-emissions for various types of large mobility vehicles.

The Essence of Toshiba

Our philosophy section highlighting company values and guiding principles

Basic Commitment Of The Toshiba Group

Committed to People,
Committed to the Future.

At Toshiba, we commit to raising the quality of life
for people around the world. ensuring progress
that is in harmony with our planet

Our Purpose

We turn on the promise of a new day.

Our Values

Do the right thing. Look for a better way.
Always consider the impact. Create together.