Toshiba’s Technology Allows Safe & Simple Means for Wireless Charging Systems for Electric Buses

  • Reduced electromagnetic interference in wireless charging systems for

    electric buses

  • Technology enables utilization of wireless charging system within limits of the

    Radio Act of Japan

Toshiba has developed a method to enable a safe and simple means for frequently recharging batteries in electric buses through wireless power transfer. Toshiba’s technology has also enabled these power transfers within the limits of Japan’s Radio Act. This was achieved by reducing electromagnetic interference (EMI) from wireless rapid charging systems for electric buses.

Benefits of wireless power transfer

  • Electricity can be transferred remotely without cables.
  • Charging of electric buses become hassle-free as they are able to charge themselves while parked or as passengers are boarding.
  • Energy can be exchanged more freely like information.

Limitations of current wireless rapid charging systems for electric buses

The wireless charging systems used to charge the batteries of electric buses utilize an 85 kHz frequency band, which is becoming the standard for wireless charging systems for electric vehicles, and deliver power at 44 kW.

The magnitudes of radiated EM waves for this high-power class of conventional wireless charging systems will become ten times larger than the specified EMI limits for the 85 kHz band, thus obtaining approval as an Industrial Facility Emitting Radio Waves under Japan’s Radio Act has been assumed to be difficult so far.

Toshiba’s wireless power transfer solution

Suppressing radiated waves is thus an important requirement to realize wireless charging systems for electric buses. Toshiba’s technology achieves this by employing two discrete 22-kW blocks that transfer power in opposite phases, cancelling EM waves from each other and reducing undesirable EM waves.

Employing this technology reduces the strength of the EM field 10m away from the device, to one-tenth or less of its unreduced strength, enabling 44 kW power transfers within the limits of the Radio Act.

This wireless charging solution has been proven through a field test campaign with actual operation of two electric buses in a joint project with Professor Yushi Kamiya of Waseda University. The joint project is commissioned by Japanese Ministry of the Environment.

How Toshiba’s technology works

  • Interference coupling between the two blocks causes variation in the magnitude and phase of the radiated EM waves, degrading the cancellation effect.
  • Identifying the optimal positioning of the two blocks to minimize interference between them is thus essential.
  • Rotating the relative position of the two blocks on a plane will eventually cause interference coupling to reach zero.
  • A theoretical analysis and an EM field simulation are used to find the relative angle at which this happens, realizing interference suppression between the two blocks.
Highlights Available in these languages (PDF) »

More News in Toshiba

Enquiry for
Toshiba’s Technology Allows Safe & Simple Means for Wireless Charging Systems for Electric Buses

Enquiry for

This field is for validation purposes and should be left unchanged.

Enquiry for

Business Strategy

Committed to People, Committed to the Future.

The Asia Pacific region is an important market for Toshiba, with one of the fastest-growing demands in infrastructure, energy, mobility, and connectivity.
Message from Managing Director

Securing Sensitive Information with Quantum Key Distribution

At Toshiba, we’re committed to delivering world leading technology that protects the private information of citizens and organizations.

Discover how Toshiba cutting edge quantum technology can protect the sensitive information of financial institutions.

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

Solutions Map - A data-connected society by Toshiba

Solutions map illustrating Toshiba’s vision for a connected data-driven society

Navigate the interactive solution map to witness the full scope of Toshiba’s integrated solutions. By connecting data across systems, we deliver comprehensive, tailored outcomes for a smarter and more sustainable future.

Our Contributions - Sustainable Activities

Technology Spotlight

Toshiba Power Semiconductor

Toshiba leverages its 60 years expertise in power semiconductors to drive automotive electrification and sustainability, offering innovative solutions to enhance efficiency and reduce emissions across industries.

Quantum Key Distribution (QKD)

Building a quantum-secure future with Toshiba’s Quantum Key Distribution

Toshiba's Commitment to a Carbon-Neutral Future

With innovative technologies and a deep commitment to building a better world, Toshiba is working towards stable, efficient green energy infrastructures for a Carbon-Neutral Future.

Superconducting Motor

Toshiba Superconducting Motor has revolutionized the airline and transportation industries. It is lightweight, compact and high-Power, making it possible to replace fossil-fuel-driven engines and contributing to zero-emissions for various types of large mobility vehicles.

The Essence of Toshiba

Our philosophy section highlighting company values and guiding principles

Basic Commitment Of The Toshiba Group

Committed to People,
Committed to the Future.

At Toshiba, we commit to raising the quality of life
for people around the world. ensuring progress
that is in harmony with our planet

Our Purpose

We turn on the promise of a new day.

Our Values

Do the right thing. Look for a better way.
Always consider the impact. Create together.