Permanent Magnet Synchronous Motor (PMSM)

Toshiba started developing the PMSM system in the early 1990s. Utilising data accumulated through R&D and field tests, Toshiba established the PMSM main circuit system technologies for railway cars.

The most strong point of PMSM system is High efficiency. There is no secondary copper loss, decreased primary copper loss, iron loss and others. Overall loss, drastically reduced to less than 50% compared to induction motor.

Permanent Magnet Synchronous Motor (PMSM)

Key Features

Energy icon

Energy Efficiency

Energy icon

Reliability

Noise icon

Low Noise

Maintenance icon

Easy Maintenance

High Efficiency

Permanent Magnet Synchronous Motor (PMSM)
High-efficiency chart for Permanent Magnet Synchronous Motor PMSM
* 1The motor efficiencies were calculated with loss measurement based on IEC 60349-2 at the temperature below 40oC from 8/25/2009 to 9/25/2009 for PMSM.

Energy Savings

** This graph compares the energy consumption measurement result on the following condition.

Trains used:

C151 PMSM train:

EMU131/132 of SMRT fleet which equips PMSM propulsion system

C151 Existing train:

EMU 109/110 of SMRT fleet which equips DC motor propulsion system

Duration:

7th Dec 2015 to 11th Dec 2015 (Total 5 weekdays)

Running pattern:

These 2 trains were used in commercial operation and they run in a series as possible as diagram allows.

Energy savings comparison under specific conditions

Energy Savings

C151 PMSM Train Running Mileage

Since the introduction of C151 PMSM prototype train (2 train-sets) in July 2015, C151 PMSM trains (total 6 train-sets) keep to run with no service disputation disruption.

Energy savings of C151 PMSM train over running mileage

Easy Maintenance

Toshiba has developed a totally-enclosed structure to make maintenance operations smarter compared to our conventional Induction Motor (IM) in terms of cost and time.

We have succesfully eliminated potential internal contamination, which makes cleaning no longer required through the PMSM’s service life. We have also engineered a structure allowing the bearing unit to be replaced without disassembly of the entire motor.

Easy maintenance feature for simplified servicing and upkeep
Easy maintenance feature for simplified servicing and upkeep
Product Enquiry

Enquiry for
Permanent Magnet Synchronous Motor (PMSM)

This field is hidden when viewing the form

Enquiry for

This field is for validation purposes and should be left unchanged.
This field is hidden when viewing the form

Enquiry for

Business Strategy

Committed to People, Committed to the Future.

The Asia Pacific region is an important market for Toshiba, with one of the fastest-growing demands in infrastructure, energy, mobility, and connectivity.
Message from Managing Director

Securing Sensitive Information with Quantum Key Distribution

At Toshiba, we’re committed to delivering world leading technology that protects the private information of citizens and organizations.

Discover how Toshiba cutting edge quantum technology can protect the sensitive information of financial institutions.

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

QKD finance section highlighting secure quantum-based financial solutions

Monetary Authority of Singapore (MAS) Advisory on Addressing the Cybersecurity Risks Associated ...

Solutions Map - A data-connected society by Toshiba

Solutions map illustrating Toshiba’s vision for a connected data-driven society

Navigate the interactive solution map to witness the full scope of Toshiba’s integrated solutions. By connecting data across systems, we deliver comprehensive, tailored outcomes for a smarter and more sustainable future.

Our Contributions - Sustainable Activities

Technology Spotlight

Toshiba Power Semiconductor

Toshiba leverages its 60 years expertise in power semiconductors to drive automotive electrification and sustainability, offering innovative solutions to enhance efficiency and reduce emissions across industries.

Quantum Key Distribution (QKD)

Building a quantum-secure future with Toshiba’s Quantum Key Distribution

Toshiba's Commitment to a Carbon-Neutral Future

With innovative technologies and a deep commitment to building a better world, Toshiba is working towards stable, efficient green energy infrastructures for a Carbon-Neutral Future.

Superconducting Motor

Toshiba Superconducting Motor has revolutionized the airline and transportation industries. It is lightweight, compact and high-Power, making it possible to replace fossil-fuel-driven engines and contributing to zero-emissions for various types of large mobility vehicles.

The Essence of Toshiba

Our philosophy section highlighting company values and guiding principles

Basic Commitment Of The Toshiba Group

Committed to People,
Committed to the Future.

At Toshiba, we commit to raising the quality of life
for people around the world. ensuring progress
that is in harmony with our planet

Our Purpose

We turn on the promise of a new day.

Our Values

Do the right thing. Look for a better way.
Always consider the impact. Create together.